Coaxial Connectors at Farnell

Coaxial Connector, Coaxial Connectors, pc connectors and other connectors from industry-leading manufacturers, in stock and ready to ship today.
At Farnell we offer an extensive range of Coaxial Connectors from the industries leading manufacturers.
Coaxial connectors are used as a transmission line for radio frequency signals. These types of connectors are typically found in applications such as connecting radio transmitters and receivers with their antennas, computer connections and the distribution of cable television signals.
One advantage of coaxial connectors over other types of transmission line is that in an ideal coaxial cable the electromagnetic field carrying the signal exists only in the space between the inner and outer conductors. This allows coaxial cable runs to be installed next to metal objects such as gutters without the power losses that occur in other transmission lines, and provides protection of the signal from external electromagnetic interference.
Farnell offers flexible ordering, with immediate dispatch through a choice of channels and delivery options to suit individual requirements. Take advantage of our wide choice of products and high quality service today to help you make the right design choices.
Click here for the full Coaxial connector range from Farnell >>