Farnell stocks R&S MXO4 series for effortless EMI Debugging
The R&S MXO 4 Series Oscilloscope from Rohde & Schwarz delivers a number of industry firsts including the world’s fastest real-time update rate and a once-in-a-decade ASICS engineering breakthrough offering accelerated insights.
Farnell is now stocking Rohde & Schwarz (R&S) MXO 4 Series, the first in the next generation of oscilloscopes.
Its fast acquisition rate, high vertical resolution, and sensitive trigger enable engineers to capture more signal details and isolate events with greater precision. The instrument provides the world’s fastest real-time update rate of more than 4.5 million acquisitions per second. This rate enables development engineers to see more signal detail and infrequent events than any other oscilloscope, providing an unparalleled understanding of physical layer signals and faster testing.
The R&S®MXO 4 Series excels in both performance and value. The R&S®MXO 4 spectrum function has the familiar interface of a spectrum analyzer making it the ideal solution for EMI debugging. The spectrum measurement setup dialog offers basic spectrum analyzer parameters such as start and stop frequency and resolution bandwidth.
The R&S MXO 4 Series features a 13.3” full-HD capacitive touchscreen and an intuitive user interface. The instrument’s small footprint, very low audible noise, VESA mounting and rackmount kit for installation makes it an ideal oscilloscope for any engineering workspace
Key benefits for engineers include:
- World’s fastest acquisition rate of over 4.5 million waveforms/s and industry’s lowest trigger rearm time of < 21ns to see signals faster
- 12-bit ADC vertical resolution, 18-bit architecture with HD mode, minimal noise of 104 and ±5 V offset range with 500 µV/div sensitivity to see signals accurately
- Standard memory of 400 Mpoints per channel with option for 800 Mpoints to capture more time
- Industry's most sensitive trigger of 1/10 000 div enables the isolation of events with greater precision, making it easier for engineers to identify anomalies and potential issues in their signals
The new R&S MXO 4 oscilloscope series is available from stock at Farnell in EMEA.
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7. With more than 80 years of experience, 47 localised websites, and a dedicated team of over 3,500 employees, Farnell provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Farnell in Europe, Newark in North America, and element14 in Asia Pacific. It also sells direct to consumers through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com/