Global distribution agreement signed between Farnell and Alliance Memory
Alliance Memory’s products are now available to Farnell customers worldwide
Farnell, has signed a global distribution agreement with Alliance Memory, bringing a significant new supplier to Farnell’s semiconductor portfolio. The new agreement will further expand Alliance Memory’s market reach through Farnell’s customers worldwide.
The complete range of Alliance Memory’s SRAM, DRAM, embedded multi-media card (eMMC), and flash memory ICs will now be available for fast delivery from Farnell. These memory products meet market needs in the communications, computing, consumer electronics, medical, automotive and industrial markets.
This agreement means Alliance Memory's legacy memory devices will be supplied through Farnell's long-established distribution network and customer base, enhancing their availability and simplifying the procurement process.
The Alliance Memory product range includes:
SRAM
- A full range of 3.3V and 5V asynchronous SRAMs used with mainstream digital signal processors (DSPs) and microcontrollers
- Low-power SRAMs, pseudo-SRAMs
DRAM
- 3.3V synchronous DRAMs (SDR)
- Mobile DDRs, 2.5V single (DDR1), 1.8V double (DDR2) and 1.5V and 1.35V triple rate (DDR3), 1.2V quadruple rate (DDR4/DDR4X) synchronous DRAMs
Flash ICs
- 5V/3.3V/1.8V Parallel NOR Flash
- 1.8V & 3.3V Serial NOR Flash (SPI / DUAL / QSPI / Multi IOs),
- 1.8V & 3.3V SLC Serial NAND Flash (SPI / DUAL / QSPI / Multi IOs),
- 1.8V & 3.3V SLC Parallel NAND Flash (SPI / DUAL / QSPI / Multi IOs)
Farnell parent company Avnet is an existing authorised distributor of Alliance Memory products, which means that Farnell customers will benefit from Avnet’s existing Alliance Memory ecosystem that delivers design, product, marketing and supply chain expertise for customers at every stage of a product development lifecycle.
Alliance Memory's memory products are designed to meet the customers’ specific needs who require drop-in replacements for discontinued or obsolete memory components. Alliance Memory has earned a reputation for delivering reliable solutions to extend the life of existing systems and equipment without costly redesigns or requalification.
Jose Lok, Farnell Global Product Category Director, Semiconductors, said: “This welcome introduction of Alliance Memory’s extensive memory solutions to our global line card will help our customers worldwide to avoid redesign costs when going through end-of-life transitions for legacy products. Alliance Memory has remained finely tuned to market trends and has expanded its DDR3 SDRAMs, eMMC and other product ranges to ensure the demand for these solutions can be met.”
Alliance Memory’s memory solutions are now available from stock at Farnell in EMEA, Newark in North America and element14 in APAC.
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production, Farnell helps its customers access the products and services they need 24/7. With more than 80 years of experience, 47 localised websites, and a dedicated team of over 3,500 employees, Farnell provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Farnell in Europe, Newark in North America, and element14 in Asia Pacific. It also sells direct to consumers through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com/